Part Number: AMC1200
Hello All.
I have bought this amplifier but reading the datasheet there is something that I don't understand. Is posible to control de gain? I know that the max differential input is +-250mV and the output will be 5[V]-0 with a voltage reference of 2.5[V]. So, As the ampliffier is linear if the input is 125 mV so the output will be 3.75[V] - 1.25[V] with a voltage reference of 2.5[V]. It's correct?