Other Parts Discussed in Thread: ADS1278, THS4031, PGA281, OPA177, THS4521
Hello,
Could i connect directly Vo1 and Vo2 outputs of the PGA204 into one of the differential inputs of ADS1278/4 ?
Thanks in advance.
Francis.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Errol,
I need gain of 1000.
What are the max output current & resistance of the Vo1 & Vo2 outputs ?
Is it necessary or better to insert THS4031 between Vo1/2 outputs and differential analog inputs of the ads1278 (PGA281 datasheet, page 25, figure 50) ?
Best,
Francis.
Hi Francis,
are you using only a fixed gain of 1000? If that is the case, it is not necessary to use a programmable gain instrumentation amplifier, but like Errol already mentioned a dual channel precision op amp instead.
Regarding the max output current & resistance of the Vo1 & Vo2 outputs: page 8 in the datasheet specifies the output current limit with the short circuit current as shown in the attached figure.
You should consider using a buffer amp between your gaining op amp and ADS1278 for a maximized and reliable data acquisition.
Some thoughts about buffer designs are mentioned in this application report.
Regards,
Miriam
Hi Miriam,
Thanks for your answer.
For me this figure was for the Vo output, so you say that it's for the Vo1/2 outputs too ?
i have choose the PGA204 because he needs less external components, i have strain gauge and i don't have to sort resistances for the gains.
But if you have a reference to propose, i am open :O).
Regards.
Francis.