our project requirement is as below
want to measure input AC current and AC voltage which is having a frequency of 4Mhz, it's a sinusoidal input
isolation I feel can be provided by a transformer(i doubt the 4MHz frequency of input will do anything ?)
after its isolated from input, i want to pass it through a bridge rectifier to measure the ac voltage rms and power rms
kindly suggest me the approach to be followed, i did not see any high bandwidth AC input power monitor or current monitor
Regards