Part Number: LM5056A
Hello,
Regarding to the LM5056, my customer is asking some question.
(Question)
(1) For example , when LM5056 is power off(Vdd=0) and Vin(Vin_K,SENSE,OUT) =60V ,
is there any problem on LM5056?
From ABSOLUTE MAXIMUM RATINGS, I think that there will be no problem.
My understanding is correct?
(2) What purpose is VAUX used for?
Is it possible to make unused? If so, how does it connect as unused pin?
(3) About SMBus,
They will use MCU with I2C for SMBus.
In this case, is it possible to unused SMBA pin?
If so, is SMBA pin opened?
Regards,
Tao2199