Part Number: XTR111
Hi,
I have some problems to understand the device and the neccesary short circuit protection, the function of the external short circuit is no problem.
I thought that the device will limit the output current as a function of Vin.
So for example If I have Vin = 2V, Rset = 2K I will get an output current of 10mA, independent of the load.
If I have a load of 1Ohm , the outout current should be still 10mA. So why do I have to limit the output current ?
Kind regards