Part Number: DRV401
Other Parts Discussed in Thread: OPA552, DRV411
Dear Technical Support Team,
Do you have an example for external compensation coil driver?
I'd like to know what type of external amp should I select and example schematic, what point I should take care of.
■Summary of requirement.
・large and small compensation coil (1000 turn / 18Ω)
・Shunt register is 10Ω
・primary current is applied 50A , then Icomp pin flows 50mA between 10 pin and 11 pin is expected, so buffer output current should be 50mA.
・External Driver is supplied ±15V power.
→I think high current output amp is better like OPA552.
Best Regards,
ttd