Part Number: LMC6001
When using the LMC6001 for high precision applications, is there a preferred PCB material that minimizes amplifier input leakage current? The design will utilize a 6-layer board with two internal ground planes and paying a higher price for a material other than FR-4 is acceptable. Also, is cutting slots in the board (minimizing PCB contact area around the trace) a sufficient substitute to air wiring the input (as shown in the datasheet layout guidlines)?