Other Parts Discussed in Thread: TINA-TI, AFE031
AFE031 , Analog Front End for DC PLC (power Line Communication) has a TINA simulation schematic , but there is no documentation available on how to use this file in TINA-TI . I've gone through the data sheet of AFE031 which also has a DAC but this simulation does not include any DAC and some pins of AFE031 are also missing in the TINA simulation or have different pin names.
I need to implement a PLC over a 24V DC line. i already have encoded data and only need the analog front end , as a POC i'm trying to simulate this situation using the given TINA file.
any documentation or help on configuring the two AFE031's available in the simulation as Tx and Rx and inputting encoded data?
thanks in advance.