Other Parts Discussed in Thread: LMV393-N, TLV1701, TLV7011, TLV3201, LMV393, LMV7239
Hi team,
The customer has two questions for LMP7300.
Q1: The datasheet shows ""For precise level detection applications, TI recommends symmetric hysteresis values less than 5 mV to 10 mV."
on page 12. For the customer's application, the hysteresis value is 100mV. Can LMP7300 meet his requirement?
If not ,would you recommend a suitable device? How to determine the hysteresis value for the comparator devices?
Q2: The datasheet shows "By optimizing overdrive, the pullup resistor and capactive load fault update rates of 200 kHz to
250 kHz or greater can be achieved." on page 10. Now the customer's switching frequency is higher than 500KHZ.
Can LMP7300 meet his requirement? If not ,would you recommend a suitable device?
Best Wishes,
Mickey Zhang
Asia Customer Support Center
Texas Instruments