This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OPA2320-Q1: 150 degrees C parameters

Part Number: OPA2320-Q1


Hi,

 this device has operational temp range up to 150 degrees C, but all parameters are tested and guaranteed only up to 125 degrees.

Do we have any characterization/data in the range from 125 to 150 degrees?

If not, it is better to specify the device in the tested range only.

Thanks

Umberto

  • Umberto,

    We do SPECIFY the device up to 125C and additionally provide OPERATING temperature range but these two ranges have different meaning.

    All of our products, including OPA2320-Q1, have two temperature ranges: specified range and operational range BUT we test in production or otherwise guarantee meeting of datasheet max/min parameters limits only for specified temperature range - see datasheet table condition column for various specs.  

    Having said that, we do characterize most of the op amp parameters up to 150 deg C - all datasheet graphs show -40C to 150C temperature range - which assure that the part will operate like an op amp up to 150C but it may not meet the datasheet max or min limits above 125 C.