Other Parts Discussed in Thread: OPA337, OPA191, TINA-TI, OPA140
Hello, I am looking for help designing a charge amplifier that has very low input impedance. My basic circuit design looks like this:
Here, R1 is a many-turn coil (200-100 turns, depending on the wire gauge) about 8 inches in diameter with resistance from 3 ohm to 130 ohm. In this application, I am changing the magnetic field near the coil, which then generates a current in the coil. I want to integrate that current to find the total charge that flows in the coil. I expect around 0.5 to 3 nC. However, the magnetic field takes about 1 s to change, so I have been using C1 = 30 nF and R2 = 30 Mohm. That combination of R1 and R2 produces a lot of noise when there is no signal in the coil. Is there a good amplifier that will work for my application?