Other Parts Discussed in Thread: OPA277, INA116
I am having trouble understanding the circuit design needed to build a pH monitor. I have researched previous threads dating back to 2012 and the Spec sheet. My ignorance is hampering my ability to understand certain aspects of the historical posts.
1. Can I use my Adruino's 5V tap to power the INA121 or do I have to use +V/-V power supply?
2. From what I have read since my pH sensor outputs a +/- mV, I can set Vref to be added to the sensor's output to offset it output to a positive voltage range as required for my Arduino's ADC ports? Am I correct?
3.Can I use my Adruino's 5V tap to supply a voltage divider using 1% Resistors to provide Vref to INA121 or must I use only an additional OA's output to supply Vref?
4. Per the spec sheet's page 9 Figure 3 discussion I need to provide a input bias current path. Should I use Fig 3's Ceramic Transducer example for my pH sensor set up or the Thermocouple example?
5. Should I include the spec sheets page 11 Figure 9 addition OPA277 and the Capacitor & Resistor? If so I am confused does the frequency = 1/2PI*R*C indicate that signal noise is cut off Below or Above this frequency?
Thanks