Hi,
I was considering a design as shown below where the THS4271 amp drives the AC input (80MHz, 50mVpp sine wave) to an LC bias tee composed of a 2.2uH inductor and 100nF capacitor. DC is assumed to be driven by an ideal DC power supply via the inductor, and AC by the THS4271 amp via the capacitor.
The output of the bias tee (ie the AC+DC summed output) is connected to a time variable resistor represented by "VCR_1K" below. The resistance profile of this variable resistor is assumed to vary sinusoidally at 500MHz with a peak to peak value of 6 ohmspk-pk and average value=9ohms.
Can the THS4271 amp be expected to drive this AC load successfully resulting in say at least 40mVpp ripple amplitude at the bias tee output, especially considering the fast transient current requirements posed by the sinusoidally varying variable load?
NOTE: The end application intended is a power supply ripple rejection test circuitry, wherein the DC supply with AC ripple is to be applied at the DUT supply. The voltage variable resistance is intended to mimic the DC and transient current requirements of the DUT. Normally we use standard 50E output resistance signal sources to drive the AC input of the bias tee, but with fast switching transient current requirements of the DUT it poses a lot of limitations in satisfying the transient current requirements especially because we remove the DUT supply decaps for this test.
The intent here is to attempt to use a buffer stage to do away with the 50E output resistance and hopefully be able to supply the fast transient current requirements better with the lower output impedance of the buffer.
Thanks,
Anoop