Part Number: OPA846
Background:
I am using an OPA846 in a transimpedance amplifier with ~100 kOhm of gain. There is a resistor equal to the gain resistor connected to the non-inverting input to cancel the DC offset caused by the input bias current. This lowers the common mode input voltage significantly.
Question:
The datasheet states 10uA as the typical input bias current and 21uA as the maximum over temperature. Are there graphs of the distribution of the input bias current over temperature? I am looking for something similar to FIGURE 15 in the datasheet but for input bias current over the operating temperature range.
Thanks