Hi Team,
I’d like to find one operational amplifiers to replace ST TSX711A but with wider supply voltage range. I just find OPA189DBV on the website. while, it's only preview.
Can you suggest one replacement?
thanks,
Bell
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Bell,
I have a couple of different recommendations for you depending on what device specifications may be of greatest interest to you.
OPA192 - 36V supply, wider 10 MHz bandwidth, low input offset voltage (25 µV max) and drift (0.15 µV/°C), 1 mA quiescent current draw
OPA227 - 36V supply, wider 8 MHz bandwidth, low input offset voltage (75 µV max) and drift (0.1 µV/°C), low 3 nV/√Hz broadband voltage noise
The OPA192 is the lower power alternative of the two, with the OPA227 offering better noise performance - both offer a significant improvement in DC and AC performance over the TSX711 with wider 36V supply ratings.
Please let me know if you have any questions on the above devices or have any additional design constraints we should take into consideration.
---
Christopher Stemple
Product Marketing - Precision Amplifiers
Hi Bell,
One additional recommendation I wanted to run by you - the OPA196. It gives up some bandwidth compared to the OPA192 and OPA227, but uses significantly less power while improving DC performance over the TSX711, and is more comparable in terms of price as well.
Please let us know if we can answer any additional questions.
--
Christopher Stemple
Product Marketing - Precision Amplifiers