Part Number: BUF602
Other Parts Discussed in Thread: TINA-TI, BUF602, THS4031, THS3491
Tool/software: TINA-TI or Spice Models
Hello, Dear TI expert,
I have a design, it is very similar to the fig 1 in sboa065. I don't have very clear requirement yet, I guess the gain is around 4. input is 0.5V, the load is 50ohm. the bandwidth is 40Mhz.
can I use BUF602 and THS4031 replace buf and opamp in the figure 1.
and made a simulation of the circuit.
my questions are,
1, is this design make sense?
2, if I need increase gain to 8 and want 40MHz bandwidth, THS4031 is not good enough, what is the recommendation of the OP AMP.
Appreciate your help.
David Sun
seems PDF attachments not work, only png shows up.