Part Number: THS4011
Other Parts Discussed in Thread: DAC8871, OPA211A
Hello,
Can be left floating the power pad of THS4011?
Currently the customer use OPA211A for the buffer of the DAC8871 output.
Then the settling time from +10V to -10V is not better than the datasheet figure.
In the following post, the THS4011 is recommended to replacement from the OPA211A.
Since the OPA211A has not power pad, there is no layout for thermal pad.
This question is related to the following E2E post.
https://e2e.ti.com/support/data_converters/precision_data_converters/f/73/p/622084/2296640
Best Regards,
Ryuji