Other Parts Discussed in Thread: OPA684, OPA2684, OPA695, VCA824
Hi,
for my project thesis I'm using the AD9952 which creates a sine wave output. After rf-transformer and filter the signal amplitude should be 1V.
Now I want to go down to 0.1V with a voltage divider and then on demand go up to 4,5V with switchable resistors.
The problem is the high frequency of max 100MHz.
So the amplification of the OPamp should reach from 1 to nearly 100 in the range from 0 to 100MHz.
The output should deliver enough current for 50 Ohm impedance matching.
I have a dual power supply of +5V and would be great if it the amp was offset compensated.
Does anybody know a suitable device for this application?
Thanks.
Peter