Part Number: LMC6484
The datasheet states an input voltage range of (V-) - 0.3 to (V+) + 0.3.
The datasheet also states a maximum current at input pin of +/- 5mA and note3 refers "Limiting input pin current is only necessary for input voltages that exceed absolute maximum input voltage ratings."
Does the current limit rating infer that the maximum input voltage can be exceeded as long at the current limit is not exceeded?
Many Thanks
"