This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TL074: Possibility of damage by accident

Guru 19655 points
Part Number: TL074


By customer mistake, TL074's feedback resistor was not connection (open).

Is this case have possibility of TL074 damage?

【Background】

・Circuit is attached above.(Vcc is ±15V)

・At second time, feedback resistor properly connect 10kΩ, but output is abnormal.

・I want to know possibility of damage TL074, because should judge TL074 failure or external cause on abnormal output.

Best regards,

Satoshi