A related question is a question created from another question. When the related question is created, it will be automatically linked to the original question.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
The lowest power op-amp with a shutdown is the TLV2760 (28uA @ 500kHz), though it is 3.6V max. The next lowest would be the TLV2450 (42uA @ 220kHz, lower noise)
The LPV/TLV8xx series were designed for always-on applications. The current is low enough it can easily be powered off a GPIO pin.