Part Number: TLV333
Other Parts Discussed in Thread: TLV2333
Hi Team,
Could you help to confirm the supply current when the chip is operating?
Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hey Daniel,
This answer will depend on the amount of channels you have on your device. For the one channel TLV333 with a supply voltage between 1.8V to 5.5V you can expect the typical supply current to be 17uA and max to be 28uA. With the two channel TLV2333 this number would double and with the four channel device, this number is 4 times the single channel value.
Section 7.7 on page 8 of the datasheet. Quiescent current is the same as supply current.