This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM324: output changes after few days

Part Number: LM324

I am using LM 324 as current to voltage converter for high current(10A=1.1V)

when I set the output using potentiometer it works perfectly fine. but slowly the output starts decreasing over period of days -

that is after 5- days the output drops to 1.04 V from 1.1 V - input remaining constant

what can be the reason? how to avoid this?