Dear TIers,
I would like to generate one pair signals, phase difference is 180 degree, <1MHz, the amplitude stability is about 1uV.
Thanks very much!
BR
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear TIers,
I would like to generate one pair signals, phase difference is 180 degree, <1MHz, the amplitude stability is about 1uV.
Thanks very much!
BR
Hello user3677382:
The best approach is to use a fully-differential operational amplifier (FDA); especially, if you need a precise 180-degree difference between the outputs. TI has a full line of FDA products. You can find more information here:
The FDA products are supported on the High-Speed Amplifiers e2e forum.
Regards, Thomas
Precision Amplifiers Applications Engineering