Part Number: LM397
Other Parts Discussed in Thread: TL331, LM339
Hello team,
Customer had several issues on LM397 device (DC1649) during In Situ Test. Indeed, they noticed a shift on the Output_Low which exceeds the 400mV limit (with a pull up 5V, 500Ohms). The transistor saturates. With 4.8V, the issue does not occur.
It is interesting to notice that, in the past, the average output voltage was about 300mV and has recently increased to 480mV.
So, do you think that something during manufacturing step could justify this shift? (die/fab changing for example).
Thank you for your help.
Best regards