Other Parts Discussed in Thread: ADS1115
I would like to be able to reasonably accurately measure electrochemical probes with an ADS1115. The LMP7721 looks good, but is there a less expensive option that would still allow me to amplify the current in the +/- 1V range? Since the ADS1115 only measures 0-5 +V is there anything special I will have to do to measure the +/- 1V from the probes?
Edit:
Prior discussion at ADS1115: AMP for pH and ORP Probe Interface
Also, the ADS1115 measures differential measurements to get bipolar readings, so all voltages have to be positive with reference to ground. It has four inputs, so I would hope to be able to connect at least two probes per ADS, but if I tied all of the reference signals to the same pin, perhaps I could measure three probes?