Hi dear supporting team,
if customer need add input filter for INA240, is there uplimitation for the shunt cap value? could they add 0.1uF? (will it affect the stability?) tks a lot!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Mayrim,
thanks for the answer!
so why couldn't the cap be lower than 0.1uF? TKS A LOT!
Hi Vera Mao,
That cap can be as low as you want it, those are only recommended values.
Note: this is recommended for DC signals. I just discussed with the application designer of this device, he say he do not recommend using filtering if your have PWM signal.