Other Parts Discussed in Thread: LMP8640HV, INA240
Hi, I'm unable to find a TI equivalent op amp to the LT6016. The main feature that I'm interested in is the "Over-The-Top" input stage. Meaning that the input protection diodes will activate at a certain voltage whether the op amp is powered on or off. For example, with the LT6016, the input protection diodes will active at approximately 80V above or -25V below to Vs-. This op amp will be used for precision filters and signal conditioning. Input signal can range anywhere from 10uVp to 3mVp with a max bandwidth of 1MHz. Does a similar TI op amp exists?
Thank you.