This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TL441: What is the actual minimum Vcc(+/-)?

Part Number: TL441

Hi there. I see on the datasheet for the TL441 LOG Amp that the Vcc max is +/- 8V but it doesn't list the minimum. Most example circuits show a value of +/-6V. My question is will it work at +/-3V and what is the actual minimum voltage?

The general chip schematic kind of suggests that it could work at +/- 3V but I'm only estimating a guess. ;)

Thanks...