Part Number: INA139
Other Parts Discussed in Thread: INA240
I have two questions about INA139. The first one is : Can i use the INA139 with a differential input voltage range from 100mv and 1.5V? How does it operate in this situation?
The second one is related to my design that doesn't work (figure above). I test the circuit in a real pcb situation. The input is a 24V ramp with 100us of trise. At the output, i have a delayed signal while the input is OK. Why do i have this behaviour? (figure below) output is the blue one, the other two are the differential input:
Thank you very much.
Regards