This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV3541: I can't simulate TLV3541 with P-SPICE.

Part Number: TLV3541


I downloaded the TLV3541 spice model from the homepage and simulate to P-SPICE.

However, the following error occurred and simulation was not possible.


ERROR(ORPSIM-15108): Subcircuit VCCS_EXT_LIM used by X_U16.XVCM_CLAMP is undefined

ERROR(ORPSIM-15108): Subcircuit VCCS_LIM_IQ used by X_U16.XIQp is undefined

ERROR(ORPSIM-15108): Subcircuit VCCS_LIM_IQ used by X_U16.XIQn is undefined

ERROR(ORPSIM-15108): Subcircuit VCCS_LIM_CLAWp used by X_U16.XCLAWp is undefined

ERROR(ORPSIM-15108): Subcircuit VCCS_LIM_CLAWn used by X_U16.XCLAWn is undefined

ERROR(ORPSIM-15108): Subcircuit CLAMP_AMP_LO used by X_U16.XCL_AMP is undefined

ERROR(ORPSIM-15108): Subcircuit OL_SENSE used by X_U16.XOL_SENSE is undefined

ERROR(ORPSIM-15108): Subcircuit CLAMP_AMP_LO used by X_U16.XCLAW_AMP is undefined

ERROR(ORPSIM-15108): Subcircuit VCCS_LIM_4 used by X_U16.XCL_SRC is undefined

ERROR(ORPSIM-15108): Subcircuit VCCS_LIM_3 used by X_U16.XCLAW_SRC is undefined

ERROR(ORPSIM-15108): Subcircuit CLAMP_AMP_HI used by X_U16.XGR_AMP is undefined

ERROR(ORPSIM-15108): Subcircuit VCCS_LIM_GR used by X_U16.XGR_SRC is undefined

ERROR(ORPSIM-15108): Subcircuit VCCS_LIM_1 used by X_U16.XVCCS_LIM_1 is undefined

ERROR(ORPSIM-15108): Subcircuit VCCS_LIM_2 used by X_U16.XVCCS_LIM_2 is undefined

ERROR(ORPSIM-15108): Subcircuit VCVS_LIM_1 used by X_U16.XU1 is undefined

There seems to be a problem with the simulation model.
How do I run simulations in P-spice?