Other Parts Discussed in Thread: INA333, OPA335, TINA-TI, TIPD209, OPA388, OPA320, ADS1258-EP, ADS1258
OPA2388 or INA333.
For a prototype project i need to Measure the IR radiation (Long wave and Short wave radiation) of the environment (radiation from sun).
The Thermopile specification as follows, Sensitivity: 5 micro volts / watts meter -2, Impedence: 700 Ohms, Range : 0 to 700 watts meter -2, Response time: 2 Sec. The thermopile output may range from 0 to 3500 micro volts.
I need to design a Pre-Amplifier, Signal Conditioner and Amplifier with Low pass filter for this input. I have decided to use OPA2388 or INA333 as these have very low drift and low offset voltage. And the out put of the Amplifier is fed to an ADC (single Supply (+5Volt) 24 bit Sigma Delta ADC).
Please suggest an amplifier circuit for the above.
Thanks in advance.