Support Path: /Product/Help with Device Selection/Amplifier/filter solution/
Hi there,
I need some help choosing the right schematic / OpAmp.
I'm getting 2 single ended current sensor signals:
a) 15...2000nA
b) 0...-120nA (negative!)
That's all the information about it.
Power Supply is 24V
The job is to form the sum of the 2 signals and scale it to 10V (2000nA -> 10V)
First approach:
TIA (50V/mA too much?), Inv. Amplifier (x10), Diff.-Amplifier
Second approach:
2 shunts of 100 Ohm, Instrumentation Amplifier, amplifying the (2000nA * 100 Ohm + (-120nA) * 100 Ohm)
The Output is digitized by an given DAQ System (<= 1kHz)
Which one is the better approach?
Which parts could be used?
Thank you in advance