Part Number: LMC6772
The specs for the LMC6772 under "Absolute Maximum Ratings" mentions "Current at Output Pin ±30 mA" . Does this mean that this is the maximum current sinking ability? Also, why "+/-" ? The device can only sink current, not supply.
Also, under "Short Circuit Sinking" graph shows about 35mA at 12V. Short what? If (on state) I were to short the drain to 12V I would expect the drain current to go much higher than 35mA, and the device would probably not survive very long.
It's all a little confusing. Please explain.
Thank you.