I have a question.
Please see INA 226 data sheet p.3 【Shunt voltage gain Error vs Temperature】.
-------------------------------------------------------------------- -------------
[DataSheet]: << www.tij.co.jp/.../ina226.pdf >>
Shunt voltage gain Error vs Temperature
TYP 10 [ppm / ° C.]
MAX 50 [ppm / ° C]
-------------------------------------------------------------------- -------------
In 【SHUNT INPUT GAIN ERROR vs TEMPERATURE】 on page 6, a negative slope is shown in the range of + 25 ° C or less around + 25 ° C, and a positive slope is shown in the range of + 25 ° C or more.
It seems to be contradictory compared to TYP: 10 [ppm / ℃] shown in the table on page 3, which is correct?