Hi,
This question relates to application note sboa061.pdf, "DESIGNING PHOTODIODE AMPLIFIER CIRCUITS WITH OPA128"
I'm interested to understand the bias part of the photodiode circuit, figure 4.  There is an error in the circuit diagram I think -  the bias supply for the photodiode is currently marked as ground.  Presumably both the resistor and the 0.1uF capacitor are connected to the bias supply?  It should be obvious but I can't quite see the function of the resistor and capacitor, so hesitate to guess (and wonder what value to use for the resistor).  
 Wouldn't  the circuit still function if those components were omitted, and the photodiode connected directly to a bias supply, and also have less noise?
Thanks, Peter