Hi,
My customer is using OPA569 to drive a TEC in a bridge tied load configuration, as shown on Fig 20 in the data sheet. Vcc=5V. Vset = 2.5V.
Question: How should Vm (the other end of the current monitor resistor) be terminated? Should it be tied to 1/2 Vcc? Should it be tied to the output of the other amplifier so that Vm is at the same potential as the opposite side of the TEC, as the data sheet suggests?
Thanks,
Rick