This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

INA128: Questions about the Supply Range

Part Number: INA128

Dear TI,

I would like to inquire about the INA128 when it is activated as below.

1)Availability in the INA128UA (-5V to 24V) range.

2)Alternative products available in the INA128UA (-5V to 24V) range.

Thank you.

  • Dear TI,
    The INA128 is used to construct a differential amplifier circuit to measure the voltage between cells
    1) INA128UA When the power supply voltage is ± 15V, please inquire whether the voltage of 15V or more can be output by differential in input
    EX) + Input side: 20V, - Input side: If 15V is input, is it the part where 5V differential output can be checked?
    2) INA128IA Power Supply Voltage is between -5V ~ 24V Is the above inquiry part measurable?
  • Hi,

    This post has been answered here: e2e.ti.com/.../639604