This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TL971: TL971 output decreased when connect to LDO

Part Number: TL971


Dear;  

When the TL971 doesn't connect TPS76301, the output of TL971 is normal, but when it connected to the input of TPS76301, the output of TL971 is decreased to 1V and its waveform is distortion. Could you please give me some advice? Please refer to the attached circuit.

Best regards

Kailyn

  • Hi Kailyn,
    Please provide DC voltage measurements at MIC2+, VDD_6V, MIC1_OUT, U11 pin 3, and the op amp output in both configurations (these can be tested with no input signal). Additionally, oscilloscope images at these nodes in both configurations should help confirm the issue.