I am planning to use the INA240 for current sensing in a BLDC motor control application. The output of the INA240 needs to swing between 0 and 3V, centered around 1.5V. Is it possible for me to run the INA240 off a 3V reference and use the reference pins to center the output at 1.5V? The INA240 specifications are listed for a supply of 5V - how much do the specifications degrade if I run from 3V?
My alternative is to just run the INA240 from a 5V supply and use a 1.5V reference input to the reference pins.