Part Number: DRV401-Q1
Other Parts Discussed in Thread: DRV401, DRV421
i had developed a current sensor A-sample with DRV401, and after the function test ,i found some questions below:
1.the current test range was too small ,it 's about ±150A. but the test range i expected was ±600A, which factors i can change to expand the test range?
2.the linearity was great at room temperature, it's about ±0.1%,but when it was exposured at 125℃, the linearity increased to about 1.5%. it was so bad. how to optimize the temperature drift? thanks very much.