Part Number: LM833-N
Other Parts Discussed in Thread: LM833
Hi,
I just built a x1000 low noise amplifier based on Fig.2 of "Design of ultra low noise amplifiers" by Vojtěch Janásek, using an LM833.
It works perfectly but the noise is 100 times what I expected based on calcs and Spice simulations, output noise is -88dBv. After trying many things I finally measured the noise at the output of the spare amp which is connected as a voltage follower (pins 6 & 7 linked and pin 5 connected to 0v). It was about 500nV/root-Hz (-125dBv). This was measured using the amplifier of which it is a part, sadly. The noise on 0v is unmeasurable (with my equipment) and the power supplies are pretty quiet as well, on the order of -140dBv.
Does the noise spec of LM833 degrade at lower supply voltages? It is only specified at +/-15v.
Regards, John.