Part Number: INA129
Other Parts Discussed in Thread: INA121
One of the circuits I’m working on has a current input signal derived from an external sensor device with a signal range of 0 to 66.6mA full scale.
I need to turn this into a 4-20mA signal, for which, I’m using an INA129 as a trans-impedance amp with an input shunt resistor to derive a full-scale input voltage of 5V to the amp, which is passed through an LPF per the sketch below:
I’ve used this LPF circuit before with INA121’s and would like confirmation that there is no issue with using the same LPF configuration with 129’s.
The gain of the 129 is set at 2 giving a 0V to 10V output swing.