This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OPA2313: Is there a dual channel op-amp with inverting/non-inverting inputs swapped?

Part Number: OPA2313


Hello,

   I have a board being built where I'm using a OPA2313IDGKR dual channel op-amp but I made a mistake and swapped the -IN and +IN pins. Is there any dual-channel op-amp in this VSSOP-8 footprint that have these two pins reversed? It's used in a basic voltage-follower configuration, powered from +5V.

   I realize it's a long shot, but I thought it's at least worth asking, in case someone else has had to do this before.

Thanks,

Derek