Part Number: LM8261
Hello,
Our customer use the LM8261.
The condition of the customer using as follows.
Voltage follower circuit
V+=12V , VIN=VOUT=10V
Load: 60uF capaitor
Current limit resistor: 5 ohm
When the power up and power down, it occur inrush current.
It is nearly short circuit condition.
It is a less than 1.5msec and there's no heat up.
Is there any problem?
Best Regards,
Naoki Aoyama