Part Number: INA333
Other Parts Discussed in Thread: OPA2320, ADS1131
Thank you for the forum. I want to make a strain gauge interface. I seem to find oodles of different devices to do this. For my use I already have a micro with a ADC having a good 16 bit, DIFFERENTIAL INPUT capability with plenty of speed on tap. I just need a little GAIN. 100 maybe.
Looking at front end "IN" amplifiers like the INA333 and hoping to find one that has a differential output, single supply with simple OCM setting capabilities seems missing... Either I'm missing something literally or conceptually. Conceptually meaning -- there must be a good reason that this is not more prevalent as a BRIDGE BUFFER - ADC DRIVER
Full bridge ( 4 strain gauges 350 ohms each )
3 or 5 volt excitation.
Expecting about 20mV full scale from bridge
The mid bridge voltage being exactly excitation/2
I'd like to have at least 12 of my bits not wiggling around. (I'm in a fairly low noise environment. )
I see some differential input and output amplifiers
But don't seem to make the STRAIN GAUGE application connection with any of them.
Their claim to fame seems to be " these drive differential input ADC's great!"
Am I off base?
Appreciate any helpful responses.
Thanks