I have a very simple circuit.
Comparator, 9V single supply, Vinput = 0..3V square signal, Tr,Tf < 100ns.
see below
The output has an overshoot of 0.5V and a "drop" down to 1V on the rising edge. the load is only 1K.
if I remove the 1k, the "drop" disappears, but the overshoot stays.
Is this a phase reversal problem?
I have tried changing Rf to 1K , it did not help.
any suggestions?