Part Number: OPA2192
I have some question about OPA2192.
In the situation the power of OPA 2192 is OFF.
How to prevent damage to the OPA 2192 when applying an external voltage to the output pin (pin 1) of the OPA 2192?
For data input pins on the data sheet, it is stated that the input current should be ±10 mA or less.
However, I could not find a description about output pins.
If the current of the output pin is suppressed to ± 10 mA or less,(Insert a resistor between output pin and external power supply)
Will OPA 2192 receive no damage?
Kind regards,
Taka