Part Number: INA126
Other Parts Discussed in Thread: INA122, , ADS1115, LM7705, OPA320
I've got a 2 wire pyranometer. It generates voltage 0-40mV based on the strength of the solar irradiation.
I've got in my toolbox INA126 and INA122.
Are they the right devices to boost the 0-40mV output?
If I understood the data sheets, the inputs can be from -0.7V to 0.7V, is that correct?
Kind regards
Dean