Part Number: INA333
Other Parts Discussed in Thread: OPA333
Hi,
I am working through a setup trying to simulate noise in the INA333 using TINA. I have already gone through and calculated the results by hand but wanted to run a simulation for verification. I am not getting the expect output for the noise spectral density or Total noise graphs.
I did some searching online and found this presentation on the exact topic I was looking for. I worked through the results got a matching answer by hand but when trying to simulate I run into a number of issues.
My Circuit is the following image and I have included my TINA file.
Issues:
1) If I do not have R8 (100K) on Vout then TINA reports issue with U1.Q21 "Operating point not found".
This resistor was not there in the linked ppt presentation but was there in the INA333 Tina file downloaded from the web.
2) Once adding R8 the issue changes to U2.D17 "Operating point not found".
I then removed the OPA333 circuit setting the Vref CM to mid-supply and just used a voltage source.
3) Finally the Noise analysis will run but only if I set "Analysis>>Mode>>"Single". The TINA comments in blue specify to use "analysis>>Mode>>"Parameter Stepping" but will not run in this mode.
Once running in the "single mode" I get a different response from the presentation on slides 30 and 31.
An image of my Total noise graph looks as follows:
The graph for noise spectral density is also very different. I initially thought it had to do with Log scale on axis but once I changed the axis to match I still had different results.
To summarize: I would like to know if it looks like I am missing a step when trying to simulate noise in the ina333. I have an identical circuit to the one in the linked presentation but cannot repeat the results.